SD card support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SD card support

Jump to solution
2,977 Views
jimschimpf
Contributor II

Is there a library for the M0 processors (eg LPC11xx) that runs an SD card and supports the FAT file system ?

0 Kudos
Reply
1 Solution
2,793 Views
jimschimpf
Contributor II

Thank you I am studying your code, there is enough code that I hope I will be able to muddle through the Chinese.

--jim schimpf

View solution in original post

0 Kudos
Reply
3 Replies
2,794 Views
jimschimpf
Contributor II

Thank you I am studying your code, there is enough code that I hope I will be able to muddle through the Chinese.

--jim schimpf

0 Kudos
Reply
2,793 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Jim

If your problem is solved, please help us mark the correct answer to close this question, thank you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
2,791 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Jim Schimpf,

   I have a LPC1114 project which contains SD and FATFS,  the comment is all wrote in Chinese, but it doesn't matter, you can refer to the code directly.

Wish it helps you!

If you still have problem, please contact me!

0 Kudos
Reply