SD/MMC Questions

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SD/MMC Questions

1,719 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by bunrockter on Sat Aug 04 13:43:37 MST 2012
I recently got the Hitex board and I am trying to get the SD peripheral up and running. I have chose not to use the driver the comes with the 4350 because I am using a state based design, and I want to tightly integrate it with a state machine.

I have looked at the code, and set up my initialization accordingly. I get and interrupt for card presence, but I am unable to get a Remote timeout or command done interrupt to fire. I am trying to send the idle command to the card (which I know doesn't respond) but I would expect to get a command done interrupt & I don't.

Is setting up the args register, and setting the START_CMD bit in the CMD register all I have to do to send a command?

Thanks
标签 (1)
0 项奖励
回复
1 回复

1,707 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mirfan on Mon Sep 24 05:43:03 MST 2012
Hi bunrockter,

Is the START_CMD bit getting cleared after you set the CMD register? CIU clears this bit once it accepts the command.

Thanks
0 项奖励
回复