SCimer Input Capture in LPC546xx Interrupt is not getting?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SCimer Input Capture in LPC546xx Interrupt is not getting?

Jump to solution
2,565 Views
TPN_CHN
Contributor II

Dear Sir,

i am SCTimer Input capture implemented in LPC54628 EVK Board

following code developed using config tool ( Pins & Peripherals Init ) but interrupt does not occurs why?

Please suggestion where is mistake in my code, please help me sir.

// Pin_mux.c

void BOARD_InitBootPins(void)
{
SCTimer_InitPins();
}

/* clang-format off */
//* FUNCTION ************************************************************************************************************
*
* Function Name : SCTimer_InitPins
* Description : Configures pin routing and optionally pin electrical features.
*
* END ****************************************************************************************************************/
/* Function assigned for the Cortex-M4F */
void SCTimer_InitPins(void)
{
/* Enables the clock for the input muxes. 0 = Disable; 1 = Enable.: 0x01u */
CLOCK_EnableClock(kCLOCK_InputMux);
/* Enables the clock for the IOCON block. 0 = Disable; 1 = Enable.: 0x01u */
CLOCK_EnableClock(kCLOCK_Iocon);

INPUTMUX->SCT0_INMUX[0] = ((INPUTMUX->SCT0_INMUX[0] &
/* Mask bits to zero which are setting */
(~(INPUTMUX_SCT0_INMUX_INP_N_MASK)))

/* Input number to SCT0 inputs 0 to 6.
* : 0x00u. */
| INPUTMUX_SCT0_INMUX_INP_N(0x00u));

const uint32_t SCT0_IN0 = (/* Pin is configured as SCT0_GPI0 */
IOCON_PIO_FUNC4 |
/* Selects pull-up function */
IOCON_PIO_MODE_PULLUP |
/* Input function is not inverted */
IOCON_PIO_INV_DI |
/* Enables digital function */
IOCON_PIO_DIGITAL_EN |
/* Input filter disabled */
IOCON_PIO_INPFILT_OFF |
/* Standard mode, output slew rate control is enabled */
IOCON_PIO_SLEW_STANDARD |
/* Open drain is disabled */
IOCON_PIO_OPENDRAIN_DI);
/* PORT0 PIN24 (coords: M7) is configured as SCT0_GPI0 */
IOCON_PinMuxSet(IOCON, SCTIMER_INITPINS_SCT0_IN0_PORT, SCTIMER_INITPINS_SCT0_IN0_PIN, SCT0_IN0);
}

// Peripheral.c file

const sctimer_config_t SCT0_initConfig = {
.enableCounterUnify = false,
.clockMode = kSCTIMER_System_ClockMode,
.clockSelect = kSCTIMER_Clock_On_Rise_Input_0,
.enableBidirection_l = true,
.enableBidirection_h = false,
.prescale_l = 0U,
.prescale_h = 0U,
.outInitState = (uint8_t)(SCT0_OUTPUT_1),
.inputsync = (uint8_t)(SCT0_INPUTSYNC_0)
};
uint32_t SCT0_event[1];

static void SCT0_init(void) {
SCTIMER_Init(SCT0_PERIPHERAL, &SCT0_initConfig);
/* Initialization of state 0 */
SCTIMER_CreateAndScheduleEvent(SCT0_PERIPHERAL, kSCTIMER_InputRiseEvent, 0, kSCTIMER_Input_0, kSCTIMER_Counter_L, &SCT0_event[0]);
SCTIMER_SetupCounterStartAction(SCT0_PERIPHERAL, kSCTIMER_Counter_L, SCT0_event[0]);
/* Interrupt vector SCT0_IRQn priority settings in the NVIC. */
NVIC_SetPriority(SCT0_IRQN, SCT0_IRQ_PRIORITY);
/* Enable interrupt SCT0_IRQn request in the NVIC. */
EnableIRQ(SCT0_IRQN);
SCTIMER_StartTimer(SCT0_PERIPHERAL, kSCTIMER_Counter_L);
}


/***********************************************************************************************************************
* Initialization functions
**********************************************************************************************************************/
void BOARD_InitPeripherals(void)
{
/* Initialize components */
SCT0_init();
}

/***********************************************************************************************************************
* BOARD_InitBootPeripherals function
**********************************************************************************************************************/
void BOARD_InitBootPeripherals(void)
{
BOARD_InitPeripherals();
}

// main.c file

/*

/**
* @file LPC54628_Project_SCT0_IN0.c
* @brief Application entry point.
*/
#include <stdio.h>
#include "board.h"
#include "peripherals.h"
#include "pin_mux.h"
#include "clock_config.h"
#include "LPC54628.h"
#include "fsl_debug_console.h"
/* TODO: insert other include files here. */

/* TODO: insert other definitions and declarations here. */

/*
* @brief Application entry point.
*/

void SCT0_IN0_IRQ(void)
{
uint32_t Counter =0;
SCTIMER_ClearStatusFlags(SCT0, kSCTIMER_Event0Flag);

Counter = SCT0->CAP[0];
Counter = 0;
}

 

int main(void) {

/* Init board hardware. */
BOARD_InitBootPins();
BOARD_InitBootClocks();
BOARD_InitBootPeripherals();
#ifndef BOARD_INIT_DEBUG_CONSOLE_PERIPHERAL
/* Init FSL debug console. */
BOARD_InitDebugConsole();
#endif

PRINTF("Hello World\n");

/* Force the counter to be placed into memory. */
volatile static int i = 0 ;
/* Enter an infinite loop, just incrementing a counter. */
while(1) {
i++ ;
/* 'Dummy' NOP to allow source level single stepping of
tight while() loop */
__asm volatile ("nop");
}
return 0 ;
}

Advance Thanks

 

Labels (2)
0 Kudos
Reply
1 Solution
2,543 Views
nxf77486
NXP TechSupport
NXP TechSupport

Hello,

Please find the AN11538 that contains some code examples that can help you out on the configuration. Please let me know if this was helpful.

SCTimer/PWM cookbook  

View solution in original post

2 Replies
2,544 Views
nxf77486
NXP TechSupport
NXP TechSupport

Hello,

Please find the AN11538 that contains some code examples that can help you out on the configuration. Please let me know if this was helpful.

SCTimer/PWM cookbook  

2,463 Views
TPN_CHN
Contributor II

Dear Sir,

Thank you sir,

SCTimer Input Capture is working fine.

Tested with 1 mSec to 1000mSec duration.

Thanks

0 Kudos
Reply