SCTIMER Capture for LPC54018

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SCTIMER Capture for LPC54018

1,833件の閲覧回数
my22668595
Contributor I

Hi,

I used lpc54018 pwm sctimer multi state pwm sample project, how can I get the time that between Falling edge and Rising edge?

The during time from Falling edge to Rising edge is saving in SCT0->SCTCAP[] or SCT0->SCTCAPCTRL[] register?

If not,which register is the during time?

Thanks.

ラベル(1)
0 件の賞賛
返信
1 返信

1,451件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello chris wu ,

SCT match value register "SCTMATCH" and SCT match reload value register "SCTMATCHREL" .


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信