SCT input detecting rising edge

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SCT input detecting rising edge

1,162 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by temp88 on Thu Mar 24 06:20:54 MST 2016
Hello,

i'm using LPC43xx, and i need to count the number of rising edge of an external signal.
i'd like to use SCT register for counting those edge (the signal is fast).
i have some problem on setting up the chosen sct pin as input, or in finding some example code with sct timer used as input.
Regards.
Labels (1)
0 Kudos
Reply
1 Reply

1,122 Views
lpcware
NXP Employee
NXP Employee
bump
0 Kudos
Reply