SCT input detecting rising edge

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SCT input detecting rising edge

1,191件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by temp88 on Thu Mar 24 06:20:54 MST 2016
Hello,

i'm using LPC43xx, and i need to count the number of rising edge of an external signal.
i'd like to use SCT register for counting those edge (the signal is fast).
i have some problem on setting up the chosen sct pin as input, or in finding some example code with sct timer used as input.
Regards.
ラベル(1)
0 件の賞賛
返信
1 返信

1,151件の閲覧回数
lpcware
NXP Employee
NXP Employee
bump
0 件の賞賛
返信