SCT input detecting rising edge

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SCT input detecting rising edge

1,206 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by temp88 on Thu Mar 24 06:20:54 MST 2016
Hello,

i'm using LPC43xx, and i need to count the number of rising edge of an external signal.
i'd like to use SCT register for counting those edge (the signal is fast).
i have some problem on setting up the chosen sct pin as input, or in finding some example code with sct timer used as input.
Regards.
标签 (1)
0 项奖励
回复
1 回复

1,166 次查看
lpcware
NXP Employee
NXP Employee
bump
0 项奖励
回复