SCT counter. Difference use bottom/upper half.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SCT counter. Difference use bottom/upper half.

1,977 Views
jirisvabik
Contributor I

Hi guys. I have a problem with SCT counter. When I use the lower 1/2 to generate a pulse, everything works OK. When I use upper 1/2, output is dumb. What's the difference? Who bit I forget set up?

void InitCppm(void)
{
Chip_SWM_MovablePinAssign(SWM_SCT_OUT0_O, ); /*GPIO P0_0*/
Chip_SCT_Init(LPC_SCT);

Chip_SCT_Init(LPC_SCT);

Chip_SCT_Config(LPC_SCT, SCT_CONFIG_16BIT_COUNTER );

Chip_SCT_SetMatchCountH(LPC_SCT, SCT_MATCH_0, 0x9F00);
Chip_SCT_SetMatchReloadH(LPC_SCT, SCT_MATCH_0, 0x9F00);

Chip_SCT_SetOutput(LPC_SCT, SCT_OUTPUT_0, SCT_EVT_0 );
Chip_SCT_ClearOutput(LPC_SCT, SCT_OUTPUT_0, SCT_EVT_1);


Chip_SCT_Output(LPC_SCT, SCT_EVT_0);

Chip_SCT_EventState(LPC_SCT, SCT_EVENT_0, ENABLE_STATE0);
Chip_SCT_EventControl(LPC_SCT, SCT_EVENT_0, (CHIP_SCT_EVENTCTRL_T)( SCT_EVECTRL_MATCH0 |
SCT_COMBMODE_MATCH |
SCT_HEVENT_H |
SCT_STATELD_1 |
SCT_STATEEV_1 ));

Chip_SCT_EventState(LPC_SCT, SCT_EVENT_1, ENABLE_STATE1);
Chip_SCT_EventControl(LPC_SCT, SCT_EVENT_1, (CHIP_SCT_EVENTCTRL_T)( SCT_EVECTRL_MATCH0 |
SCT_COMBMODE_MATCH |
SCT_HEVENT_H |
SCT_STATELD_1 |
SCT_STATEEV_0 ));

LPC_SCT->LIMIT_H = 0x00000003;

Chip_SCT_ClearControl(LPC_SCT , SCT_CTRL_HALT_H);
}

0 Kudos
Reply
3 Replies

1,882 Views
jirisvabik
Contributor I

I found it. In function Chip_SCT_EventControl need added | SCT_OUTSEL_H

0 Kudos
Reply

1,882 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Jiri Svabik,

I'm glad to hear that you had already solved this issue, if you have any question, just feel free to contact with me.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,882 Views
jirisvabik
Contributor I

Thank you for your insights and ideas. JS

0 Kudos
Reply