SCT counter. Difference use bottom/upper half.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SCT counter. Difference use bottom/upper half.

1,878件の閲覧回数
jirisvabik
Contributor I

Hi guys. I have a problem with SCT counter. When I use the lower 1/2 to generate a pulse, everything works OK. When I use upper 1/2, output is dumb. What's the difference? Who bit I forget set up?

void InitCppm(void)
{
Chip_SWM_MovablePinAssign(SWM_SCT_OUT0_O, ); /*GPIO P0_0*/
Chip_SCT_Init(LPC_SCT);

Chip_SCT_Init(LPC_SCT);

Chip_SCT_Config(LPC_SCT, SCT_CONFIG_16BIT_COUNTER );

Chip_SCT_SetMatchCountH(LPC_SCT, SCT_MATCH_0, 0x9F00);
Chip_SCT_SetMatchReloadH(LPC_SCT, SCT_MATCH_0, 0x9F00);

Chip_SCT_SetOutput(LPC_SCT, SCT_OUTPUT_0, SCT_EVT_0 );
Chip_SCT_ClearOutput(LPC_SCT, SCT_OUTPUT_0, SCT_EVT_1);


Chip_SCT_Output(LPC_SCT, SCT_EVT_0);

Chip_SCT_EventState(LPC_SCT, SCT_EVENT_0, ENABLE_STATE0);
Chip_SCT_EventControl(LPC_SCT, SCT_EVENT_0, (CHIP_SCT_EVENTCTRL_T)( SCT_EVECTRL_MATCH0 |
SCT_COMBMODE_MATCH |
SCT_HEVENT_H |
SCT_STATELD_1 |
SCT_STATEEV_1 ));

Chip_SCT_EventState(LPC_SCT, SCT_EVENT_1, ENABLE_STATE1);
Chip_SCT_EventControl(LPC_SCT, SCT_EVENT_1, (CHIP_SCT_EVENTCTRL_T)( SCT_EVECTRL_MATCH0 |
SCT_COMBMODE_MATCH |
SCT_HEVENT_H |
SCT_STATELD_1 |
SCT_STATEEV_0 ));

LPC_SCT->LIMIT_H = 0x00000003;

Chip_SCT_ClearControl(LPC_SCT , SCT_CTRL_HALT_H);
}

0 件の賞賛
返信
3 返答(返信)

1,783件の閲覧回数
jirisvabik
Contributor I

I found it. In function Chip_SCT_EventControl need added | SCT_OUTSEL_H

0 件の賞賛
返信

1,783件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Jiri Svabik,

I'm glad to hear that you had already solved this issue, if you have any question, just feel free to contact with me.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,783件の閲覧回数
jirisvabik
Contributor I

Thank you for your insights and ideas. JS

0 件の賞賛
返信