Running the NXP-NCI project. Error: cannot connect to NXPNCI device

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Running the NXP-NCI project. Error: cannot connect to NXPNCI device

1,712 次查看
Gas
Contributor I

Hi All,

I worked fine in a project based on NXP-NCI_LPC55xx_example, but now in the debug session I see always :"Running the NXP-NCI project. Error: cannot connect to NXPNCI device".

I plugged OM5578/pn7150 Board.

Any help?

 

Thanks

0 项奖励
回复
3 回复数

1,680 次查看
Gas
Contributor I

Hi  victojimenez,

due to backup and copy, the Ven and Irq pins was missed. I don't know the reasons. In every case I'd solved.

Regards

0 项奖励
回复

1,671 次查看
victorjimenez
NXP TechSupport
NXP TechSupport

Thanks for sharing your findings! I'm glad to hear that you were able to solve the problem. 

Regards,
Victor 

0 项奖励
回复

1,687 次查看
victorjimenez
NXP TechSupport
NXP TechSupport

Hello, 

I apologize for the late response. Did you modify the example? If so, which changes did you make? I made some tests on my end with the example as it is and I didn't face any problems. 

Regards,
Victor 

0 项奖励
回复