Running code on LPC4330 from internal SRAM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Running code on LPC4330 from internal SRAM

1,061件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by kris_sin on Sun Feb 16 17:02:20 MST 2014
Hi guys,

I am using latest LPCXpresso 6.14 with LPCXplorer4330. So far I have run my application on SPIFI Flash but now I wanted run the code from RAM. Can someone help configure linker script, startup file to make the code run from internal SRAM? If someone has modified some basic blinky example that runs from SRAM I would realyy appreciate haring it with me and all forum viewers.
ラベル(1)
0 件の賞賛
返信
1 返信

1,001件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Mon Feb 17 05:05:26 MST 2014
Please don't post the same question more than once. I've posted a response in the other thread that you created.

http://www.lpcware.com/content/forum/running-code-ram#comment-1135347

Regards,
LPCXpresso Support
0 件の賞賛
返信