Reset max voltage when there is no supply

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Reset max voltage when there is no supply

Jump to solution
2,353 Views
n_boucquey
Contributor I

Hi,

We are trying to figure out if we can apply 5 V on the reset pin of the LPC1837JET100 even if its supply voltage is 0 V.

For other 5 V tolerant pins, the datasheet details that the max voltage is 3.6 V when there is no supply. Is it the same for the reset pin?

Many thanks in advance,

Nicolas Boucquey

1 Solution
2,252 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Nicolas Boucquey,

The power supply for IO pin and reset pin are different. There are diodes connects with VBAT which protect VBAT. Thus we don't need worry voltage on reset go to VBAT. We only need consider reset pin pad itself -- 5V tolerant is ok.

While for IO pins, there is no such diodes exist. So we define 3.6V tolerant if VDDIO doesn't exist.

pastedImage_1.png


Have a great day,
Jun Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

3 Replies
2,253 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Nicolas Boucquey,

The power supply for IO pin and reset pin are different. There are diodes connects with VBAT which protect VBAT. Thus we don't need worry voltage on reset go to VBAT. We only need consider reset pin pad itself -- 5V tolerant is ok.

While for IO pins, there is no such diodes exist. So we define 3.6V tolerant if VDDIO doesn't exist.

pastedImage_1.png


Have a great day,
Jun Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,252 Views
n_boucquey
Contributor I

Many thanks Jun Zhang.

Have a great day too.

Best regards,

Nicolas Boucquey

0 Kudos
Reply
2,252 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

You are welcome!

0 Kudos
Reply