Reset max voltage when there is no supply

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Reset max voltage when there is no supply

ソリューションへジャンプ
2,380件の閲覧回数
n_boucquey
Contributor I

Hi,

We are trying to figure out if we can apply 5 V on the reset pin of the LPC1837JET100 even if its supply voltage is 0 V.

For other 5 V tolerant pins, the datasheet details that the max voltage is 3.6 V when there is no supply. Is it the same for the reset pin?

Many thanks in advance,

Nicolas Boucquey

1 解決策
2,279件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Nicolas Boucquey,

The power supply for IO pin and reset pin are different. There are diodes connects with VBAT which protect VBAT. Thus we don't need worry voltage on reset go to VBAT. We only need consider reset pin pad itself -- 5V tolerant is ok.

While for IO pins, there is no such diodes exist. So we define 3.6V tolerant if VDDIO doesn't exist.

pastedImage_1.png


Have a great day,
Jun Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

3 返答(返信)
2,280件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Nicolas Boucquey,

The power supply for IO pin and reset pin are different. There are diodes connects with VBAT which protect VBAT. Thus we don't need worry voltage on reset go to VBAT. We only need consider reset pin pad itself -- 5V tolerant is ok.

While for IO pins, there is no such diodes exist. So we define 3.6V tolerant if VDDIO doesn't exist.

pastedImage_1.png


Have a great day,
Jun Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,279件の閲覧回数
n_boucquey
Contributor I

Many thanks Jun Zhang.

Have a great day too.

Best regards,

Nicolas Boucquey

0 件の賞賛
返信
2,279件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

You are welcome!

0 件の賞賛
返信