Request: Example code for LPC11U2X/3X of CDC using USB rom'ed driver.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Request: Example code for LPC11U2X/3X of CDC using USB rom'ed driver.

1,441 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by larsen on Mon Dec 10 03:19:32 MST 2012
We are looking for examples for CDC class using the USB ROM'ed driver for LPC11U2X, LPC11U3X.

We thought it would be simpler to use the Rom'ed drivers than using the nxpUSBlib, but without good examples as a starting point this is not the case.

Any one with a pointer to some examples?
thanks
标签 (1)
0 项奖励
回复
1 回复

1,428 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by drs on Tue Dec 11 15:57:17 MST 2012
nxpUSBlib has a switch that forces it to use the USB ROM drivers. It is in the configuration file nxpUSBlibConfig.h

There are also several non-nxpUSBlib source code examples that use the ROM drivers here: http://www.lpcware.com/gfiles/devper/lpc11Uxx
0 项奖励
回复