Replacement of SWM(Switch Matrix) in LPC55s69

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Replacement of SWM(Switch Matrix) in LPC55s69

946 Views
ravicha
Contributor II

i have code for LPC804 of UART1 and UART2 where UART1 is responsible for communication to the smart card and UART2 is for genrating the clock for smart card , this two UART used throught SWM 

now i want to replace this in lpc55s69 how to do it

1 Reply

911 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @ravicha 

USART functions are available on all LPC55S6x/LPC55S2x/LPC552x devices as a
selectable function in each Flexcomm Interface peripheral. Up to 8 Flexcomm Interfaces
are available. So you can choose two of them to use.

 

BR

Alice

0 Kudos
Reply