Replacement dongle for FTDI USB-ICP-LPC2K

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Replacement dongle for FTDI USB-ICP-LPC2K

1,401件の閲覧回数
jking2
Contributor I

Hello,

Can anyone recommend a replacement for the obsolete USB-ICP-LPC2K made by FTDI?  We use flash magic with the USB-ICP-LPC2K dongle to erase the read protect bit on an NXP LPC1787.

Thanks

ラベル(2)
0 件の賞賛
返信
1 返信

1,349件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I have checked the following documentation:

https://www.teamfdi.com/wp-content/uploads/USB-ICP-LPC2K-Master-Brochure-R11.pdf 

The USB-ICP-LPC2K device is a third party product, currently, it is obsolete. It is an USB-TO-SCI device. I think you can order the similar product from the other manufacturers.

I have searched on Google with the key words" usb to uart dongle", you can see a lot of product.

Regarding the pin and Reset pin which can force LPC17xx enter ISP mode, I think you can press the button on the target board so that the chip can enter ISP mode after power-up.

Hope it can help you

BR

XiangJun Rong

pastedImage_2.png

0 件の賞賛
返信