Remote Firmware update LPC54616 - without HW reconfiguration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Remote Firmware update LPC54616 - without HW reconfiguration

1,346 Views
sleroy
Contributor I

Is it possible to update the MCU firmware without any physical reconfiguration of the board. 

Can it be accomplished remotely and with what method?

We understand there are USB cable update methodologies which require a jumper reset.

Is there a method which would allow remote update without a Hardware reconfiguration (jumper reset).

0 Kudos
Reply
1 Reply

1,251 Views
soledad
NXP Employee
NXP Employee

Hi, 

Please check the following tool and let me know if this helps. 

Flash Magic - Welcome 

Have a nice day!

Regards

Sol 

0 Kudos
Reply