Reinvoke (ISP) not working

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Reinvoke (ISP) not working

1,766 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Lea on Sat Feb 13 00:24:55 MST 2016
I am using a LPCA 11C24 and flash new firmware over the primary CANopen bootloader.
My user app process a command to start the reinvoke function. But this causes a crash. I read in other posts that it is important to turn PLL off, set timer value to it defaults., so I modiy my ipa_reinvoke methode

<code >
/**
* @brief Prepare an invoke µC to call isp-command reinvoke
*/
void iap_reinvoke_bootloader(void)
{
static uint32_t cmd[5] = {IAP_REINVOKE_ISP_CMD,0,0,0,0};
static uint32_t result[4];

cmd[0] = IAP_REINVOKE_ISP_CMD;// reinvoke ISP command

__disable_irq();

// make sure 32-bit timer 1 is turned on before calling ISP
LPC_SYSCTL->SYSAHBCLKCTRL |= 0x00400;
//Chip_Clock_EnablePeriphClock(SYSCTL_CLOCK_CT32B1);

// make sure GPIO clock is turned on before calling ISP
LPC_SYSCTL->SYSAHBCLKCTRL |= 0x00040;
//Chip_Clock_EnablePeriphClock(SYSCTL_CLOCK_GPIO);

// make sure IO configuration clock is turned on before calling ISP
LPC_SYSCTL->SYSAHBCLKCTRL |= 0x10000;
//Chip_Clock_EnablePeriphClock(SYSCTL_CLOCK_IOCON);

// AHB clock divider must 1:1
LPC_SYSCTL->SYSAHBCLKDIV = 1;
//Chip_Clock_SetSysClockDiv(1);

// disabele PLL
LPC_SYSCTL->MAINCLKSEL = 0;// enable IRQ oscillator
LPC_SYSCTL->MAINCLKUEN = 0x01;// update MLCK clock source
LPC_SYSCTL->MAINCLKUEN = 0x00;// toggle update register
LPC_SYSCTL->MAINCLKUEN = 0x01;

while (!(LPC_SYSCTL->MAINCLKUEN & 0x01))// wait until updated
;

// reset the stack pointer to point to the top of the stack minus 32 byte for IAP
// for LPC11Cxx where top of RAM (8kB) is 0x1000_2000: MSP = (0x1000_20000 - 0x20 = 0x1000_1FE0)
//__set_MSP((uint32_t)0x100001FE0);
//__set_MSP((uint32_t)0x100002000);

/* Set stack pointer to ROM value (reset default) */
__set_MSP(*((uint32_t *) 0x100001FE0));

// the cortex M0 needs to synchronize the CPU cache
__ISB();

Chip_GPIO_SetPinDIROutput(LPC_GPIO, 0, 3);
Chip_GPIO_SetPinOutLow(LPC_GPIO, 0, 3);

Chip_GPIO_SetPinDIROutput(LPC_GPIO, 0, 1);
Chip_GPIO_SetPinOutLow(LPC_GPIO, 0, 1);

iap_entry(cmd, result);
}
<\code>

Does anyone have a tip for me, what am I doing wrong?
Labels (1)
0 Kudos
Reply
2 Replies

1,546 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Lea on Sat Feb 13 02:41:39 MST 2016
Great :D

You solve my problem. That was the reason.

Thank you very, very much
0 Kudos
Reply

1,546 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by vtw.433e on Sat Feb 13 02:28:56 MST 2016
You have changed the stack and are then calling gpio functions. I don't think that will work and is probably causing the crash. In fact you shouldn't need to change the stack as the reinvoke ISP call will reset it for you.
0 Kudos
Reply