Reinvoke ISP in USB mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Reinvoke ISP in USB mode

1,077件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpressologinname on Tue Sep 08 07:44:16 MST 2015
I'm trying to jump back into ISP mode of the rom bootloader.

This is the code I use to activate the bootloader:
DISABLE_INTERRUPT();
// Reset USB block
Chip_SYSCTL_PeriphReset(RESET_USB);
Chip_Clock_SetSysClockDiv(1);
LPC_WWDT->TC = 0xFFFFFF;
Chip_WWDT_Feed(LPC_WWDT);
// re-invoke ISP in USB
Chip_IAP_ReinvokeISP(2);

The current CDC disappears, but the massstorage device doesn't appear. Windows or Linux don't recognize the device. If I look into the device it uses PID 0000 and VID 0000. So it seems as if the descriptor isn't correctly filled in.

Anyone any ideas how to make this work?
ラベル(1)
0 返答(返信)