Reinvoke ISP (LPC1224)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Reinvoke ISP (LPC1224)

2,436件の閲覧回数
albertosavazzi
Contributor I

I'm trying to program LPC1224 using the reinvokeisp mode from user code but I'still have no answer to a sync character '?'.

void ReinvokeISP(void)
{

/* disable WatchDog */
LPC_WWDT->MOD = 0;

__disable_irq();

/* make sure 32-bit Timer 1 is turned on before calling ISP */
LPC_SYSCON->SYSAHBCLKCTRL |= (1 << 10) | (1 << 10);
/* make sure GPIO clock is turned on before calling ISP */
LPC_SYSCON->SYSAHBCLKCTRL |= (1 << 29) | (1 << 30) | (1 << 31); //0x00040;
/* make sure IO configuration clock is turned on before calling ISP */
LPC_SYSCON->SYSAHBCLKCTRL |= (1 << 16); //0x10000;

// AHB clock divider must 1:1
LPC_SYSCON->SYSAHBCLKDIV = 1;

// disabele PLL
LPC_SYSCON->MAINCLKSEL = 0;// enable IRQ oscillator
LPC_SYSCON->MAINCLKUEN = 0x01;// update MLCK clock source
LPC_SYSCON->MAINCLKUEN = 0x00;// toggle update register
LPC_SYSCON->MAINCLKUEN = 0x01;

while (!(LPC_SYSCON->MAINCLKUEN & 0x01))// wait until updated
;

// the cortex M0 needs to synchronize the CPU cache
__ISB();

LPC_GPIO0->DIR |= (1<<12); //set GPIO0_12 DIR out
LPC_GPIO0->CLR = (1<<12);

command[0] = IAP_CMD_REINVOKE;

// reset the stack pointer to point to the top of the stack minus 32 byte for IAP
// for LPC11Cxx where top of RAM (8kB) is 0x1000_2000: MSP = (0x1000_20000 - 0x20 = 0x1000_1FE0)
/* Set stack pointer to ROM value (reset default) */
__set_MSP(*((uint32_t *) 0x1FFF0000));

iap_entry(command, output);

}

Please help, I spent many days with no success.

Thanks.

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,855件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Alberto Savazzi,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.

I was wondering if you can upload the demo, then I can run the demo on the board to replicate the issue.

I'm looking forward to your reply.

Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,855件の閲覧回数
albertosavazzi
Contributor I

Hi jeremyzhou,

thank you for your help. Below you can find the link to get the little demo.

ReinvokeISP demo

0 件の賞賛
返信