Regarding the data transfer between GPIO of LPC4370 and SRAM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Regarding the data transfer between GPIO of LPC4370 and SRAM

1,488 次查看
sujayp
Contributor II

Is it possible to write a program code in keil ARM MDK 5 regarding the

Initial  instruction:-It  would be data transfer between the GPIO of the Port 6 [31 bit ] directly to the address of  the internal  SRAM and The next instruction would be increment the SRAM Address and It would be nice if it is without using the DMA configuration.

I have to write GPIO  Drivers for lpc4370FET256
will you please suggest me, how to write the same

thanks in advance


Regards
Sujay

0 项奖励
回复
1 回复

1,266 次查看
soledad
NXP Employee
NXP Employee

Hello Sujay, 

Please check the below thread and let me know if this helps!!

Running code from RAM | www.LPCware.com 

Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复