Regarding interface with thermal camera

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Regarding interface with thermal camera

2,795 Views
Vijay222
Contributor III

I have LPC55s16 board how to interface  with flir gen 3 usb thermal camera  give me some code and detail explanation for connection 

0 Kudos
Reply
5 Replies

2,764 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Vijay222 

What specific USB class for usb thermal camera ?

Thanks

Jun Zhang

0 Kudos
Reply

2,739 Views
Vijay222
Contributor III

It is usb  type c based thermal camera  to detect the temperature 

IMG-20230203-WA0004.jpgIMG-20230203-WA0004.jpg

0 Kudos
Reply

2,710 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

HI

USB Type-C is a USB interface appearance or shape standard. Not USB class

LPC doesn't have a driver code to support Flir thermal camera. In order to let LPC communicate the camera, you need to know this camera USB and I2C protocal, and the related USB class. there is SDK USB classes demo code for different USB class. You can refer it to develope your own driver.

Thanks,

Jun Zhang

 

0 Kudos
Reply

2,693 Views
Vijay222
Contributor III

I don't know how to develop the code would you help me out or give refferance codes.

0 Kudos
Reply

2,762 Views
Vijay222
Contributor III
Usb c type
0 Kudos
Reply