Regarding USB Usage in LPC4357

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Regarding USB Usage in LPC4357

1,461 次查看
sudheerkumardor
Contributor I

Dear All,

I want to use the USB in LPC4357 , for the Application of sending the large amount of data to modem , but modem class, protocol and interface are Vendor specific. so Shall I use this one as CDC class device.

if we use microcontroller as Host, is it possible to receive the data with out host request. (Any interrupt data supported by microcontroller it self). (ex: If we get any in coming call to chipset, that we will directly intimate to mcu or Host need to pool every time for any data).

Help the above questions.

Provide the USB Host drivers for LPC4357.

标签 (2)
0 项奖励
回复
1 回复

1,208 次查看
soledad
NXP Employee
NXP Employee

Hi, 

You can use LPCOpen, it includes an extensive set of examples of USB. These examples can help you as reference. 

LPCOpen Libraries and Examples|NXP 

Best Regards 

Sol 

0 项奖励
回复