Regarding USB Usage in LPC4357

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Regarding USB Usage in LPC4357

1,445 Views
sudheerkumardor
Contributor I

Dear All,

I want to use the USB in LPC4357 , for the Application of sending the large amount of data to modem , but modem class, protocol and interface are Vendor specific. so Shall I use this one as CDC class device.

if we use microcontroller as Host, is it possible to receive the data with out host request. (Any interrupt data supported by microcontroller it self). (ex: If we get any in coming call to chipset, that we will directly intimate to mcu or Host need to pool every time for any data).

Help the above questions.

Provide the USB Host drivers for LPC4357.

Labels (2)
0 Kudos
Reply
1 Reply

1,192 Views
soledad
NXP Employee
NXP Employee

Hi, 

You can use LPCOpen, it includes an extensive set of examples of USB. These examples can help you as reference. 

LPCOpen Libraries and Examples|NXP 

Best Regards 

Sol 

0 Kudos
Reply