Reg: LPC845 ADC maximum Negative Voltage to withstand.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Reg: LPC845 ADC maximum Negative Voltage to withstand.

1,719件の閲覧回数
PK_1114
Contributor II

Hai,

What is the maximum allowable negative voltage on the ADC Pin in LPC845 Micro controller operating on the +3.3V.

Thank You,

B Pavan Kumar  

タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,659件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi PK_1114 

According to datasheet, ADC anolog input limit is as below

ZhangJennie_0-1698221653986.png

It is recommended to connect an overvoltage protection diode between the analog input pin and the voltage supply pin.

Have a nice day,

Jun Zhang

0 件の賞賛
返信

1,690件の閲覧回数
PK_1114
Contributor II
Hi,

Is there any Reverse Protection in the LPC845 ADC pin, if there what is it voltage tolerance. I need to give the Sinusoidal wave to the ADC.

Thank You,
B Pavan Kumar
0 件の賞賛
返信