Reference to AN11018.....any USB Interface difference between LPC13xx and LPC15xx?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Reference to AN11018.....any USB Interface difference between LPC13xx and LPC15xx?

1,857 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by riscy00 on Sun Mar 06 23:07:53 MST 2016
In reference to AN11018

Is there difference in USB interface hardware and register layout including between LPC13xx and LPC15xx?

The LPCopen only have ROM based USB library, I'm looking for non ROM library collection that work for LPC15xx and wondering if I can use LPC13xx library for that?

R.



标签 (1)
0 项奖励
回复
4 回复数

1,791 次查看
lpcware
NXP Employee
NXP Employee
bump
0 项奖励
回复

1,791 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by DF9DQ on Tue Mar 08 06:55:02 MST 2016
There's no way you can use LPC1343 code. The USB block of LPC1549 uses a totally different concept, and you would have to completely re-write all lower layer code.
0 项奖励
回复

1,791 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by riscy00 on Mon Mar 07 22:38:19 MST 2016
so it not possible to use non-rom USB code (composite MSC+CDC) from 1343 into 1549 device.

I'm running out of option with no expert help. I unable to get MSC+CDC composition working on 1549 device. I posted code sample for 1549 expresso board which has MSC working and CDC working alone but fails on MSC+CDC composite.  
0 项奖励
回复

1,791 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by DF9DQ on Mon Mar 07 07:40:59 MST 2016
LPC15xx uses the same USB block as the LPC1345/46/47.
Note that the older LPC1343 is completely different!
0 项奖励
回复