Reading/writing SYSCON on LPC824

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Reading/writing SYSCON on LPC824

1,344件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Anemaet on Sat Mar 14 10:04:49 MST 2015
Hi all,

I have a problem with a LPC824.

Somehow I cannot read nor write the SYSCON register. Both actions crash the controller. The GDB debugger log is in the code block below.

Do I have to enable that part of the APB somehow?

Thanks so much!


Log

WARNING: Failed to read memory @ address 0x40048000
WARNING: Failed to read memory @ address 0x40048004
WARNING: Failed to read memory @ address 0x40048008
WARNING: Failed to read memory @ address 0x4004800C
WARNING: Failed to read memory @ address 0x40048020
WARNING: Failed to read memory @ address 0x40048024
WARNING: Failed to read memory @ address 0x40048030
WARNING: Failed to read memory @ address 0x40048040
WARNING: Failed to read memory @ address 0x40048044
WARNING: Failed to read memory @ address 0x40048070
WARNING: Failed to read memory @ address 0x40048074
WARNING: Failed to read memory @ address 0x40048078
WARNING: Failed to read memory @ address 0x40048080
WARNING: Failed to read memory @ address 0x40048094
WARNING: Failed to read memory @ address 0x400480E0
WARNING: Failed to read memory @ address 0x400480E4
WARNING: Failed to read memory @ address 0x400480E8
WARNING: Failed to read memory @ address 0x400480EC
WARNING: Failed to read memory @ address 0x400480F0
WARNING: Failed to read memory @ address 0x400480F4
WARNING: Failed to read memory @ address 0x400480FC
WARNING: Failed to read memory @ address 0x40048100
WARNING: Failed to read memory @ address 0x40048150
WARNING: Failed to read memory @ address 0x40048154
WARNING: Failed to read memory @ address 0x40048170
WARNING: Failed to read memory @ address 0x40048174
WARNING: Failed to read memory @ address 0x40048204
WARNING: Failed to read memory @ address 0x40048214
WARNING: Failed to read memory @ address 0x40048230
WARNING: Failed to read memory @ address 0x40048234
WARNING: Failed to read memory @ address 0x40048238
WARNING: Failed to read memory @ address 0x400483F4

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,305件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Anemaet on Mon Mar 16 01:29:59 MST 2015
Ah I figured it out, I was mixing arm-elf with arm-eabi.

This can be closed.
0 件の賞賛
返信

1,305件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Anemaet on Sun Mar 15 02:01:48 MST 2015
So my question really is, is there a way you can prevent access to SYSCON?

If there isn't this uC is bricked, otherwise I'll have a lead to solving my problem.
0 件の賞賛
返信