Reading LPC17xx flash memory via ISP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Reading LPC17xx flash memory via ISP

1,537 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ezharkov on Tue Jun 10 16:10:30 MST 2014
I'm trying to read LPC1765 flash memory via ISP IAP. Getting the correct data for everything except the first 512-bytes block. I.e., "R 512 512" works fine. But "R 0 512" returns garbage (correct reply checksum, but not the data that I expect). The same program works fine with LPC1788.
Labels (1)
0 Kudos
Reply
1 Reply

1,465 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ezharkov on Wed Jun 11 06:39:44 MST 2014
OK, this must have something to do with the boot ROM mapping. Still not clear why this works on LPC1788.
0 Kudos
Reply