Read device

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Read device

2,286 Views
zhaoqinsu
NXP Employee
NXP Employee

Two identical chips are tested on the same testbench EVB board. The result is a successful read device, the other  one can not read device.However, this chip can not read the device tests on anther EVB ,it can read again. This phenomenon is often appear, I 'm very puzzled.

0 Kudos
Reply
1 Reply

2,167 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Z.q. Su,

     Could you tell us what the LPC chip you are using? Please give use the chip part number.

    When you test on the same EVB board, did you solid it on the chip? Or use some socket?

    Please check the pin connection,  whether it has the pin bad connection problem, your problem is caused by the hardware.


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply