Read device

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Read device

2,286件の閲覧回数
zhaoqinsu
NXP Employee
NXP Employee

Two identical chips are tested on the same testbench EVB board. The result is a successful read device, the other  one can not read device.However, this chip can not read the device tests on anther EVB ,it can read again. This phenomenon is often appear, I 'm very puzzled.

0 件の賞賛
返信
1 返信

2,167件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Z.q. Su,

     Could you tell us what the LPC chip you are using? Please give use the chip part number.

    When you test on the same EVB board, did you solid it on the chip? Or use some socket?

    Please check the pin connection,  whether it has the pin bad connection problem, your problem is caused by the hardware.


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信