Read back memory from LPC55S06 by J-flash

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Read back memory from LPC55S06 by J-flash

5,004件の閲覧回数
jimmyli
Contributor V

Hi,

      We programed a hex file to LPC55S06 (official demo) by J-Flash (v7.56 or v8.82f, connecting with Jlink v9) tool at the first time, then we readed back "Entire chip" sucessfully.

      Then, we ereased chip and re-programed the chip by the same hex file; After that, we tried to read back "entire chip", but it failed.

      We tried all the configurations in J-Flash tool, but failed to read back again.

      We can't find the reason, and this problem will affect our production.

      Hope you can help us to fix it.

      Thanks very much.

jimmyli_0-1671092556972.jpeg

 ----hardware link

jimmyli_1-1671092582538.jpeg

----read back "entire chip"

 

jimmyli_3-1671092816957.png

----read back error from the second time

 

 

ラベル(1)
0 件の賞賛
返信
5 返答(返信)

4,952件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello All,

Yes,When reading an erased location, an uncorrectable error is flagged. Use the “blank
check” command to test for a successful erase.

About detail description, you can refer to:

https://community.nxp.com/t5/LPC-Microcontrollers-Knowledge/LPC55xx-Erased-Memory-State-0-or-1/ta-p/...  

 

BR

Alice

0 件の賞賛
返信

4,939件の閲覧回数
jimmyli
Contributor V
Hi Alice, Got it. Thanks for your reply.
0 件の賞賛
返信

4,983件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @jimmyli 

What image did you programed? 

How about erase? How about read sector?

And how about enter ISP mode, using Blhost to read? I ask this just want to confirm it is tool issue or MCU.

 

BR

Alice

0 件の賞賛
返信

4,964件の閲覧回数
jimmyli
Contributor V

Hi Alice,      

What image did you programed? 

hex image

How about erase? How about read sector?

Erase: J-Flash-->Target-->Manual Program-->Erase Chip

Read:  J-Flash-->Target-->Manual Program-->Read back-->Entire Chip

And how about enter ISP mode, using Blhost to read? I ask this just want to confirm it is tool issue or MCU.

using SWD interface, not by ISP mode.

 

Thanks very much.

0 件の賞賛
返信

4,974件の閲覧回数
Johnson_Ho
Contributor I

same issue: when a sector has been erasered, the j-flash can not readback the sector; the read back only works while the sector has been programed something.

0 件の賞賛
返信