RTOS and openSSL support for LPC43S67

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

RTOS and openSSL support for LPC43S67

5,380 次查看
zhouhaohua
Contributor I

what kind of RTOS has been test on LPC43S67, uC/OSII,FreeRTOS, any experience to share? where to get the A70CM Host API, so I can access A70CM for security related application, I have NXP-Cloud kits, which have A7001 and LPC43S67 on the board,

   any experience to Porting openSSL to LPC43S67 and work with A70CM?

标记 (1)
0 项奖励
回复
7 回复数

4,860 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Charlie,

Thank you for your interest  in NXP Semiconductor products and the opportunity tor serve you.

1) What kind of RTOS has been test on LPC43S67, uC/OSII,FreeRTOS, any experience to share?

   I'd like to recommend you to refer the LPCOpen library which contains some RTOS demos.

LPCOpen Software for LPC43XX|NXP 

2) Where to get the A70CM Host API, so I can access A70CM for security related application?

   As I know, if customer want to get A70 security support, they need signed a special NDA with NXP. This need check with A70 product line. Customer can check this with the distributor and you can learn the contacting information through the link below:

Distributor Network|NXP
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

4,860 次查看
zhouhaohua
Contributor I

I mean some popular RTOS like freeRTOS, don't have too much time to spend

on RTOS, need some generic one, so I can easy ported the SW

0 项奖励
回复

4,860 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Charlie,

Thanks for your reply.

Let me clarify it, the LPCOpen Software for LPC43XX|NXP contains a FreeRTOS template demo.

It can help you to get start with the FreeRTOS.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

4,860 次查看
zhouhaohua
Contributor I

Dear Ping:

How about SSL/TLS examples?

Regards

On Thu, Jan 19, 2017 at 10:03 PM, jeremyzhou <[email protected]>

0 项奖励
回复

4,860 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Charlie,

Thanks for your reply.

I haven't found these demos which is about SSL/TLS.

However you can go to Cypherbridge Systems Products & Services  to find the information you request.

Hope it helps.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

4,860 次查看
zhouhaohua
Contributor I

I am interested in using ARM mbed OS and TLS to test https not http , so I

can use it to do some https access examples, do you have similar

examples,

but I don't know what is the step to make https work

==============================

LWIP FreeRTOS TCP Echo example

Example description

Welcome to the LWIP TCP Echo example with FreeRTOS using the 18xx/43xx LWIP

MAC and PHY drivers. The example demonstrates PHY link monitoring, DHCP

client, ICMP Echo (ping) and TCP Echo (RFC 862) operation.

0 项奖励
回复

4,860 次查看
rocketdawg2
Contributor II

i could be wrong, but I think it is included with the dev board

LPC43S67-A70CM Cloud Connectivity Kit|NXP 

0 项奖励
回复