RTC calibration in LPC54608J512BD208

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RTC calibration in LPC54608J512BD208

1,609 Views
prasannanaik
Contributor III

Hi,

Can someone share the process of calibrating RTC of LPC54608J512BD208.

I am using this controller in a Protection Relay wherein timestamp of Fault needs to be shown to user accurately.

Right now the error is very high and due to cost constraints, i can't use less ppm crystal.

 

Thanks & best regards,

Prasanna

Labels (1)
0 Kudos
Reply
3 Replies

1,597 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

I'm afraid the LPC546xx has no way to calibrate the RTC. some other parts like LPC17xx has an enhanced RTC which offers a calibration option but LPC546xx doesn't have.

For LPC546xx, 32-bit Real-time clock (RTC) with 1 s resolution running in the always-on power domain. A timer in the RTC can be used for wake-up from all low power modes including deep power-down, with 1 ms resolution.

 

Have a nice day,

Jun Zhang

Tags (1)
0 Kudos
Reply

1,595 Views
prasannanaik
Contributor III

Hi ZhangJennie,

      We are at a product release stage so changing controller would be very difficult.

     I have observed error of around 30 sec in one day, what could be reason for this as i am using a 20 ppm crystal (Xc = 6pF) with load capacitances CL1,CL2 = 6pF.

 

Thanks & best regards,

Prasanna

0 Kudos
Reply

1,583 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Please refer our recommendation to design your RTC circuit.

DS:

13.5 RTC oscillator

13.5.1 RTC Printed Circuit Board (PCB) design guidelines

ZhangJennie_0-1615540171628.png

 

RTC Printed Circuit Board (PCB) design guidelines
• Connect the crystal and external load capacitors on the PCB as close as possible to
the oscillator input and output pins of the chip.
• The length of traces in the oscillation circuit should be as short as possible and must
not cross other signal lines.
• Ensure that the load capacitors CX1, CX2, and CX3, in case of third overtone crystal
usage, have a common ground plane.
• Loops must be made as small as possible to minimize the noise coupled in through
the PCB and to keep the parasitics as small as possible.
• Lay out the ground (GND) pattern under crystal unit.
• Do not lay out other signal lines under crystal unit for multi-layered PCB.

Here is our demo board reference design

ZhangJennie_1-1615540256684.png

 

Have a nice day

Jun Zhang

0 Kudos
Reply