RTC Operation in power down mode in LPC546xx Microcontroller

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RTC Operation in power down mode in LPC546xx Microcontroller

ソリューションへジャンプ
3,074件の閲覧回数
prasannanaik
Contributor III

Hi,

   I have a query regarding operation of RTC in LPC546. I want to know whether the RTC counter register (COUNT) will keep on updating or not in device power down mode (i.e no VDD only VBAT). The datasheet mentions that the . RTC module and the oscillator that drives it, runs directly from the device power pins. Does this means that the RTC counter won't be updated in device power down mode(i.e when only Vbat is present).

I have attached the sceenshot of the datasheet for reference.

Thanks and best regards,

Prasanna

ラベル(1)
0 件の賞賛
返信
1 解決策
2,987件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Prasanna,

You are right, the RTC counter register (COUNT) will keep on updating in device power down mode (i.e no VDD only VBAT).

BR

XiangJun Rong

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,988件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Prasanna,

You are right, the RTC counter register (COUNT) will keep on updating in device power down mode (i.e no VDD only VBAT).

BR

XiangJun Rong

0 件の賞賛
返信
2,987件の閲覧回数
prasannanaik
Contributor III

Hi xiangjun.rong‌,

   Thanks for your help.

    I verified the same on LPC546xx development board OM30192.

Thanks and best regards,

Prasanna

0 件の賞賛
返信