RTC Crystal Frequency on LPC1549

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RTC Crystal Frequency on LPC1549

2,888 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by celephicus on Sun Dec 07 17:37:12 MST 2014
We're confused, the LPC1500 user manual says that a RTC xtal of 32kHz xtal is required. But the Embedded Artists demo board uses 32.768kHz, in fact the LPC1700 user manual mentions this frequency as well. Come to think of it 32.000kHz xtals are not used much anywhere.

So I am assuming an error in the user manual and it is really 32.768kHz? Can someone confirm that 32.768kHz works? 
Labels (1)
0 Kudos
Reply
7 Replies

2,809 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Thu Dec 11 10:53:56 MST 2014
Hi celephicus,

Quote:
So I am assuming an error in the user manual and it is really 32.768kHz? Can someone confirm that 32.768kHz works?



Yes, I confirm, it works as mentioned by other users.
0 Kudos
Reply

2,809 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by larryvc on Tue Dec 09 18:15:47 MST 2014

Quote: R2D2
I'm using a MCP79410 on my boards, a 'real' RTC...


On the device page
Quote:
##Leap year compensated  to 2399


Hope we all make it! :)

0 Kudos
Reply

2,809 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Tue Dec 09 16:09:46 MST 2014

Quote: MarcVonWindscooting
What do you think about 'Micro Crystal Switzerland' devices like CV-3029-* ?



Is that something like  RV-3029  :quest:

http://www.microcrystal.com/images/_PDF/5_Real-Time-Clock_RV/rv-3029-c2.pdf

Unfortunately a little bit expensive  :((
0 Kudos
Reply

2,809 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MarcVonWindscooting on Tue Dec 09 15:49:09 MST 2014

Quote: R2D2
I'm using a MCP79410 on my boards, a 'real' RTC...



1uA time-keeping, only. Nice.

What do you think about 'Micro Crystal Switzerland' devices like CV-3029-* ?

Marc
0 Kudos
Reply

2,809 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Sun Dec 07 18:49:13 MST 2014

Quote: celephicus
This will hopefully stop my collegue worrying that he needs to put an external RTC on his board.



:bigsmile:

I'm using a MCP79410 on my boards, a 'real' RTC...
0 Kudos
Reply

2,809 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by celephicus on Sun Dec 07 18:38:58 MST 2014
Thank you R2D2. This will hopefully stop my collegue worrying that he needs to put an external RTC on his board.
0 Kudos
Reply

2,809 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Sun Dec 07 18:23:15 MST 2014

Quote: celephicus
So I am assuming an error in the user manual and it is really 32.768kHz? Can someone confirm that 32.768kHz works?



Yes, we can  :)
0 Kudos
Reply