ROM driver bugs documentation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ROM driver bugs documentation

2,135 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Hansi on Tue Jul 22 03:16:16 MST 2014
Hi!

I'm preparing a project for the LPC11U24 using the USB ROM driver. In the USB examples for the LPC11U37H, at several places are workarounds for ROM driver bugs, each with an identifier, e.g. artf32290, artf44835, artf32219.

The Errata Sheets for these devices don't show any information on the ROM drivers. Where can I find documentation on these bugs, ideally with information on which chip revisions are affected.

Thanks
  Hansi
Labels (1)
0 Kudos
Reply
4 Replies

1,967 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by PorkyBrain on Sun Apr 05 12:20:51 MST 2015
Looks to me like this data never got published. Any status update?
0 Kudos
Reply

1,967 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Hansi on Tue Nov 25 03:17:33 MST 2014
Hi!

Any news on that issue?

Thanks
  Hansi
0 Kudos
Reply

1,967 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Hansi on Wed Jul 23 06:01:15 MST 2014
Great, thanks!
0 Kudos
Reply

1,967 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_Support on Tue Jul 22 16:16:00 MST 2014
Hi Hansi,

Very good point!  I requested that all the issues/errata for the USBD ROM Stack be documented and published so users can track what is fixed in which versions of MCU devices (USBD ROM Stack) and USBD Library (Software stack).  I expect that this may take a couple weeks to get published.

Best regards,
-NXP Support
0 Kudos
Reply