RE:MCU Boot loader

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RE:MCU Boot loader

1,679 Views
Ananthakrishnan
Contributor I

Hello Team,

            I am an Ananthakrishnan. I am working with the LPC54113j256BD64 controller. So, I want help with the boot loader concept; my code in the internal flash (0x8000) place is there. So, I want to change the Boot Loader location code.I want to flash the code in the controller.without UART,SPI,I2C,I2S,Kindly help me.

0 Kudos
Reply
2 Replies

1,617 Views
Alex_Wang
NXP Employee
NXP Employee

Hello, @Ananthakrishnan 

        Hi, I don't understand your expression. Do you want the code of boot loader? You can redescribe the requirements in detail.

Best regards, Alex

0 Kudos
Reply

1,674 Views
Ananthakrishnan
Contributor I

i need a code

using functions 

0 Kudos
Reply