Question to listen to PC's input and store

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Question to listen to PC's input and store

1,607 次查看
Xeno
Contributor I

I've bought an LPC54S018-EVK board, and I'm trying to listen to PC's input.

So now, how can I make my board receive PC's input and store it into the board?

Is threr any demo code that I can refer to? I haven't found any in LPC54S018-EVK's SDK. 

Thanks a lot!

标签 (1)
0 项奖励
回复
4 回复数

1,595 次查看
carstengroen
Senior Contributor II

I think you need to describe your problem with a few more words....

For example, what is "PC's input" ????

Remember, we can't read your mind

 

0 项奖励
回复

1,594 次查看
Xeno
Contributor I

Sor, I'll make it clearer.

Imagine a scene, my board has a AES function that generates cipher of a given plaintext.

Now I connect my board to my PC using debug link, and I want the board to listen to PC's messages that give to the board by UART as plaintext.

And since the key for AES is generated by PUF related functions on board, I have to store the key into the board itself.

How can I meet such requirements?

0 项奖励
回复

1,566 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi 

The PUF generated key is sent to Hash Crypt engine or PRINCE through internal hardware bus. It is not readable by software. We can only get activation code (AC) which is used for PUF generating KEY. 

It's not possible to print PUF generated KEY to external.

Thanks,

Jun Zhang 

0 项奖励
回复

1,597 次查看
Xeno
Contributor I

Hello

Anyone answer my Question?

0 项奖励
回复