Q1: How to read from LPC54618 eeprom?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Q1: How to read from LPC54618 eeprom?

Jump to solution
5,604 Views
gmk1
Contributor III

By looking at eeprom SDK example, I understood that there is an api only for writing to eeprom using -

EEPROM_WritePage(...)

My requirement is now to read back the same but looks like api is not implemented for that. I wanted to write 4 to 8 my app specific bytes in eeprom to read during bootup or after reset.

What I assume is that one can use -

IAP_ReadEEPROMPage(...)
to read back the content. Is it okay to use both EEPROM_WritePage(...) and IAP_ReadEEPROMPage(...) to fulfill my requirements. If yes, how?
I also see that IAP_WriteEEPROMPage(...) function can be used in place of EEPROM_WritePage(...)
What are the suggestions?
- Gmk
Labels (4)
0 Kudos
Reply
1 Solution
5,422 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello Gmk 9

 

You can use the functions IAP_ReadEEPROMPage() and EEPROM_WritePage() without any issue.

EEPROM_WritePage needs 3 parameters to use it

 * param base - EEPROM peripheral base address.

 * param pageNum - Page number to be written.

 * param data - Data need be written. This array data size shall equal to the page size.

 

The IAP_ReadEEPROMPage() receives the following parameters.

 * param pageNumber - EEPROM page number.

 * param dstAddr  - Memory address to store the value read from EEPROM.

 * param systemCoreClock - Current core clock frequency in kHz.

 

You can refer to the SDK example "iap_eeprom", in that example the functions  IAP_ReadEEPROMPage() and  IAP_ReadEEPROMPage() are used. To write in EEPROM you can use the function you prefer.

 

Let me know if this is helpful, If you have more questions do not hesitate to ask me.

Best regards,

Omar

View solution in original post

0 Kudos
Reply
8 Replies
5,423 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello Gmk 9

 

You can use the functions IAP_ReadEEPROMPage() and EEPROM_WritePage() without any issue.

EEPROM_WritePage needs 3 parameters to use it

 * param base - EEPROM peripheral base address.

 * param pageNum - Page number to be written.

 * param data - Data need be written. This array data size shall equal to the page size.

 

The IAP_ReadEEPROMPage() receives the following parameters.

 * param pageNumber - EEPROM page number.

 * param dstAddr  - Memory address to store the value read from EEPROM.

 * param systemCoreClock - Current core clock frequency in kHz.

 

You can refer to the SDK example "iap_eeprom", in that example the functions  IAP_ReadEEPROMPage() and  IAP_ReadEEPROMPage() are used. To write in EEPROM you can use the function you prefer.

 

Let me know if this is helpful, If you have more questions do not hesitate to ask me.

Best regards,

Omar

0 Kudos
Reply
5,422 Views
gmk1
Contributor III

@Omar Anguiano

Can I use IAP_ReadEEPROMPage() or EEPROM_WritePage() during program execution?

I can observe controller is getting reset internally and that's a big problem!

How to use IAP_ReadEEPROMPage() during program execution?

0 Kudos
Reply
5,422 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello Gmk 9

 

The reset is not an expected behavior during the execution of the command. You can confirm the source of the reset with the System Reset Status Register SYSRSTSTAT. It could be helpful if you provide me the reset source so we can avoid the reset during the execution.

 

If you have more questions do not hesitate to ask me.

Best regards,

Omar

0 Kudos
Reply
5,421 Views
gmk1
Contributor III

Hi Omar, looks like controller is not getting to RST state but GPIOs are toggling during execution of EEPROM related activities.

This behaviour looks very strange. 

Any comments on this? 

0 Kudos
Reply
5,422 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello Gmk 9

Can you detail this issue? How the GPIO's are configured? Does the GPIO have the interruptions enabled?

I agree with you, it is a strange behavior since the EEPROM_WritePage and IAP_ReadEEPROMPage functions don't use any GPIO operations.

It would be helpful if you share me your configuration.

 

Best regards,

Omar

0 Kudos
Reply
5,422 Views
gmk1
Contributor III

GPIO config code below. No interrupts configured. -

void alarm_fb_gpio_init(void)
{
IOCON->PIO[3][4]= 0x00000120; 
IOCON->PIO[3][5]= 0x00000120; // Mains out of range
IOCON->PIO[3][6]= 0x00000120; // Emergency push button
IOCON->PIO[3][7]= 0x00000120; // Mains fail
IOCON->PIO[3][8]= 0x00000120; 
IOCON->PIO[3][9]= 0x00000120; 
IOCON->PIO[3][10]= 0x00000120; 
IOCON->PIO[3][11]= 0x00000120; // Backdoor-1 open
IOCON->PIO[3][12]= 0x00000120; // Backdoor-2 open
IOCON->PIO[3][14]= 0x00000120; // Spare-1
IOCON->PIO[3][15]= 0x00000120; // Spare-2

// Set as input pins
GPIO->DIRCLR[3] |= (1<<4) | (1<<5) | (1<<6) | (1<<7) \
| (1<<8) | (1<<9) | (1<<10)| (1<<11)\
| (1<<12)| (1<<14)| (1<<15);

CLOCK_EnableClock(kCLOCK_Gpio5);

// GPIO for Doors open buzzer indication
IOCON->PIO[5][0]= 0x00000120;
// Set as output pin
GPIO->DIR[5] |= (1<<0);

// GPIO for Doors open buzzer indication
IOCON->PIO[5][1]= 0x00000120;
// Set as output pin
GPIO->DIR[5] |= (1<<1);
}

0 Kudos
Reply
5,422 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello Gmk 9

The IOCON registers are well written, the SDK examples initialize the IOCON with the same values (0x120), I suggest you enable the rest of GPIO's clocks before writing in the IOCON registers.

I see that the GPIO directions are configured as an output, for making the GPIO input you can either use the function  

GPIO_PinInit(GPIO_Type *base, uint32_t port, uint32_t pin, const gpio_pin_config_t *config)

Or write:

GPIO->DIR[port] &= ~(1<<pin);

 

Let me know if this is helpful, if you have more questions do not hesitate to ask me.

Best regards,

Omar

0 Kudos
Reply
5,422 Views
gmk1
Contributor III

Thanks for the reply Mr Omar...

In "iap_eeprom" example IAP_ReadEEPROMPage() and IAP_WriteEEPROMPage() are used and not the EEPROM_WritePage().

I have done some trails before posting my query here. Below is my observation.

Combination of IAP_ReadEEPROMPage() and IAP_WriteEEPROMPage() is not working properly for me which IDK why!

On the other hand, combination of IAP_ReadEEPROMPage() and EEPROM_WritePage() is working.

You can test it by yourself.

 

I'll continue with the working solution as it serves my purpose.

Gmk

0 Kudos
Reply