Protection diodes

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Protection diodes

2,158 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by IanB on Thu Apr 16 13:22:53 MST 2015
Can someone give me the circuit diagram for the protection circuitry on a GPIO pin.
Labels (1)
0 Kudos
Reply
2 Replies

2,049 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by IanB on Fri Apr 17 03:18:29 MST 2015
Sorry, I was too vague.
What I meant to ask is for a circuit diagram of the internal protection circuitry on a GPIO pin.

These devices are 5V tolerant, so they don't have the same protection circuitry as your bog-standard CMOS, because there is no diode to Vdd. I was wondering what was there to prevent damage from positive-going spikes. Is there a zener?

Not all the family is the same as LPC11xx is 5V tolerant, and LPC12xx isn't, and it has diodes from input to Vdd.
0 Kudos
Reply

2,049 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Thu Apr 16 13:27:12 MST 2015
Google recommends Kevin  :bigsmile:

http://www.kevinmfodor.com/home/My-Blog/microcontrollerinputprotectiontechniques
0 Kudos
Reply