Programming spec of LPC11U35FBD48 and LPC11U36FBD48

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Programming spec of LPC11U35FBD48 and LPC11U36FBD48

1,745 Views
Leap_Electronic
Contributor II

Dear NXP team,

 

This is Austin for Leap Electronic.

Our customer All Point in Brazil need to add  LPC11U35FBD48 and LPC11U36FBD48 into our automated Programming System.

Please provide both of  LPC11U35FBD48 and LPC11U36FBD48 programming specification. 

The spec must has the following  information

1. The connecting diagram and instruction for the programming, included I/O pin, POWER pin, CLK pin.

2. AC/DC electrical specifications and timing for programming.

3. How to enter the programming mode process and the timing.

4. The flow and the timing for the function of Erase, Program, Read, and Protect.

5. The memory map, Option and Config for the programming.

6. The simple program for the programming.

Thanks in advance,

 

Best regards,

Austin

Labels (1)
0 Kudos
Reply
1 Reply

1,705 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Unfortunately, the LPC11U35/36 do not have EVK board.

I suppose that you can refer to the schematics of LPC11U68-EVK, which I attach it here.

You have to pay attention to the following items as a minimum system.

1)power supply pins

2)SWD connector

3)crystal design

4)ISP pins

The LPC11u35/36 has ROM code, which includes the api function to erase/program flash.

Do you want to erase/program flash with SWD port or in ISP mode, in ISP mode, you can use uart or USB port to program/erase.

BR

XiangJun Rong

0 Kudos
Reply