Programming boot code to external flash for LPC54018

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Programming boot code to external flash for LPC54018

3,483 Views
goran_lindgren
Contributor I

Hi,

I'm planing for a LPC54018 with an external flash connected on the EMC.

Is there support in the circuit for any ISP and or IAP to program an external flash?

Is there otherwise any tools with support for that? (I've looked at Flashmagic but they don't seem to support the

LPC54018-series) Do you have any sample code for building BootROM functionality?

Best Regards,

Göran

Labels (1)
0 Kudos
Reply
5 Replies

3,380 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

I suggest you refer this article of How to boot from the external flash for LPC54018  


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

3,380 Views
goran_lindgren
Contributor I

Hi,

Thanks for your answer, but that article doesn’t handle programing of external flash memories connected to the EMC as far as I can see.

Has the Segger software build in functionality to handle truly external flashes as well? (on the screen shoots I can see no reference to that or setup for that)

Regards,

Göran

0 Kudos
Reply

3,380 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

HI 

do you mean parallel nor?

By checking,  we don't have programming tool  for it.

for external memory, we suggest use spifi FLASH.


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

3,380 Views
goran_lindgren
Contributor I

Hi,

Yes, parallel nor flash.

Thanks for the information and your swift reply.

Regards,

Göran

0 Kudos
Reply

3,380 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

you are welcome!

0 Kudos
Reply