Programming an LPC4337 thru JTAG interface.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Programming an LPC4337 thru JTAG interface.

1,476 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ferovious on Thu Apr 30 16:00:23 MST 2015
Hello,
I'm debugging a board with an LPC4337 that was intended to be programmed (and I assume FLASHed using the IAP) through the JTAG interface with DBGEN tied low. Is programming it this way possible?  Most of the reference designs I have seen or read about suggest that DBGEN should be pulled high.  I appreciate any pointers, guidance, or comments.
Thanks!
Labels (1)
0 Kudos
Reply
1 Reply

1,392 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by embd02161991 on Thu Apr 30 16:27:56 MST 2015
Hi,

In LPC43xx devices, when the DBGEN pin is HIGH, the ARM debug mode is entered. This is required for debugging using JTAG.
When the DBGEN pin is LOW, JTAG BSDL is entered.

Thanks
NXP Technical Support
0 Kudos
Reply