Programming LPC4088 chip with LPC_Link2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Programming LPC4088 chip with LPC_Link2

3,007 Views
hassan_elahi
Contributor I

I have LPC4088FBD208,551 MCU and  LPC-Link2. I was wondering if there is any tutorial with a schematic for a very basic circuit like on and off LED (For both Mbed and MCUexpresso). Even a tutorial to show how I can program an LPC4088 QuickStart Board with LPC_Link2.

Labels (1)
0 Kudos
Reply
2 Replies

2,793 Views
soledad
NXP Employee
NXP Employee

Hi,

Please check the below threads,

LPC4088 QSB + LPCXPRESSO V8.2.2 + LPCLINK2 error 

https://community.nxp.com/thread/464098 

I hope this helps
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,793 Views
hassan_elahi
Contributor I

Hi,

Thanks for your reply. I saw these links before and even I email them and they told me that their circuit still doesn't work and they gave up. So I was wondering if there is a reliable schematic and direction for programming the chip.

0 Kudos
Reply