Programmability of LPC2142FBD64

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Programmability of LPC2142FBD64

2,500 Views
arsaenz
Contributor I

Hello,

Can someone confirm if the LPC2142FBD64.151 is fully programmable (outside of trimming) at the customer level? Or is it programmed at final test prior to shipment? Thank you.


Regards,

Alex

Labels (1)
0 Kudos
Reply
2 Replies

2,292 Views
Watonrin
Contributor I

I need the lpc2142 crown xti2000 hex file

0 Kudos
Reply

2,392 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @arsaenz 

 

"

1. if customer do not ask NXP or 3rd party programmed the chip, the LPC2142 should be fully programmable when customer received the chip.

2. if customer asked 3rd party programmed the chip with dedicate binary, the DISTY support the program service according to the agreement with end customer, if the LPC2142 programmed by DISTY, the silicon maybe blocked by CRP(Code Read Protection), then the LPC2142 can be programmed or not is depends on the CRP set level. Please contact the service vendor.

"

BR

Alice

0 Kudos
Reply