Program MAC Address in LPC40xx internal EEPROM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Program MAC Address in LPC40xx internal EEPROM

1,132 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by philip_champagne on Wed Dec 03 14:54:55 MST 2014
Is there a production programmer that can be used to write to the internal EEPROM of the LPC408x or LPC407x controller? We would like to store a MAC address there. Do you have any suggestions for storing a MAC Addresses while using the LPC408x or LPC407x microcontroller?
标签 (1)
0 项奖励
回复
1 回复

1,075 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by xianghuiwang on Fri Dec 19 18:03:44 MST 2014
Maybe a secondary bootloader to embed a command (via any peripheral) in your application to initiate  the EEPROM update.
regards,
0 项奖励
回复