Program MAC Address in LPC40xx internal EEPROM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Program MAC Address in LPC40xx internal EEPROM

1,170件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by philip_champagne on Wed Dec 03 14:54:55 MST 2014
Is there a production programmer that can be used to write to the internal EEPROM of the LPC408x or LPC407x controller? We would like to store a MAC address there. Do you have any suggestions for storing a MAC Addresses while using the LPC408x or LPC407x microcontroller?
ラベル(1)
0 件の賞賛
返信
1 返信

1,113件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by xianghuiwang on Fri Dec 19 18:03:44 MST 2014
Maybe a secondary bootloader to embed a command (via any peripheral) in your application to initiate  the EEPROM update.
regards,
0 件の賞賛
返信