Program MAC Address in LPC40xx internal EEPROM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Program MAC Address in LPC40xx internal EEPROM

1,214 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by philip_champagne on Wed Dec 03 14:54:55 MST 2014
Is there a production programmer that can be used to write to the internal EEPROM of the LPC408x or LPC407x controller? We would like to store a MAC address there. Do you have any suggestions for storing a MAC Addresses while using the LPC408x or LPC407x microcontroller?
Labels (1)
0 Kudos
Reply
1 Reply

1,157 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by xianghuiwang on Fri Dec 19 18:03:44 MST 2014
Maybe a secondary bootloader to embed a command (via any peripheral) in your application to initiate  the EEPROM update.
regards,
0 Kudos
Reply