Program LPC5526 via SWD using Flash Magic

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Program LPC5526 via SWD using Flash Magic

1,244 Views
RBlight
Contributor I

I need to program an LPC5526 using an MCU-LINK debug probe and Flash Magic.  I can do this with no problem in Rowley CrossStudio and MCUXpresso but Flash Magic only gives options for ISP programming over UART or USB.

RBlight_1-1672922688684.pngRBlight_1-1672922688684.png

How can I program the LPC5526 via SWD using Flash Magic?

 

0 Kudos
Reply
1 Reply

1,227 Views
RaRo
NXP TechSupport
NXP TechSupport

Hello @RBlight,

It seems there is nothing available for LPC55xx via SWD using Flash Magic. As you point out Flash Magic only gives you UART and/or USB for programming. It should appear a carpet with the option SWD, as other microcontrollers have it as option, nevertheless for LPC55xx you do not have that option.

Best regards, Raul.

0 Kudos
Reply