Product Info LPC2368FBD100

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Product Info LPC2368FBD100

1,870件の閲覧回数
AFZ
Contributor I

Hi,

we are using "LPC2368FBD100" in our board. i would like to know some development board that has this type of microcontroller.

this product is available or it is going obsolete , if yes, what is the alternative ?

may i use the supercap with VBAT pin instead of using battery ?

Thanks

 

Regards

Afz

0 件の賞賛
返信
3 返答(返信)

1,863件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello,

Recommend you choose other product ,you see this chip remains in longevity program until 2022,

also this is old part, almost not available. 

Please tell us your requirement, then we can give you some suggestion.

 

BR

Alice

0 件の賞賛
返信

1,858件の閲覧回数
AFZ
Contributor I

Hi,

 

can you please suggest an alternative ?

we prefer same footprint with almost same pin order.

same price list.

Thanks.

 

 

 

0 件の賞賛
返信

1,852件の閲覧回数
frank_m
Senior Contributor III

AFAIK, the LPC17xx controllers are mostly pin compatible to the LPC23xx. Which would be the LPC1768 in your case.

However, aside from alleged recent shortages, this series is not much younger than the LPC23xx, and might not save you for long.

0 件の賞賛
返信